CAB400M12XM3 MODULE LTSPICE SIMULATION
 
            I am simulating a DAB converter using CAB400M12XM3 modules. But the circuit doesnt work after I connect the Mid points of devices. It looks like a NETlist problem. How can I sort it?
Thank you
Comments
- 
            Thank you for your post, it has been approved and we will respond as soon as possible. 0
- 
            Hello ahmedtpkl, Can you please share a screen capture of the error you're getting? Thank you! 0
- 
            Hi Ahmed, In addition, if you could provide your LTspice simulation, I can take a look at your circuit and see what is going on. Thanks, Brian 0
- 
            Please find attached simulation file. When the midpoint of the device was connected to the transformer, all gate signals are zero. When I tried the same simulation with the discreate devices, It work fine. 0
- 
            Hi Ahmed, I should have noticed this from your screenshot, but your inductor 'L4' has an inductance value of 0 H. This is what is causing your simulation to fail. I recommend using the embedded parasitic parameters in your inductors and capacitors rather than explicitly defining the parasitics in the circuit. This method is more efficient. For example, right-click L3 and add '30m' to the series resistance field, then delete R4. Another thing - all inductors in LTspice default to a 1 mΩ series resistance. If this is not desired, make sure you specify the series resistance as 0. Finally - you have the temperature ports (TjQ1/TjQ2) all shorted together, and your 'Tc2' ports are not attached to the heat sink. This will all cause the thermal calculations to be incorrect. 0
- 
            It is working now. Thank you! 0