[FAQ-SF-4] Speedfit: Circuit Tab
Options
Urvi_Ahluwalia
Wolfspeed Employee - Contributor Level 2
In the [Circuit] tab, the user is required to enter additional specifications for the targeted converter. These specifications can vary based on the type of application or the topology selected. These circuit parameters are topology specific parameters like various inductances or capacitances and switching frequency of the system.
Please note: Power losses in the passive components are not considered in SpeedFit simulations, they are considered ideal components.
Figure 1: Circuit tab: enter topology specifications
Similar to the [Devices] tab, the acceptable range of each parameter is shown below the textbox when you click on it to edit the value.
Figure 2: Parameter range [example: 0.01 .. 20] is shown when editing the value in the textbox
Tagged:
0
Comments
-
0