SiC MOSFET compared to Si IGBT/Diode
we are asked to develop a power module for a high-speed compressor application. The customer is requesting a high switching frequency in the range of 12-16kHz. Output current 300A and 1200V.
· what are the benefits of SiC MOSFET compared to Si IGBT/Diode in these applications.
I am new to SiC do you have some information to share for me to learn or understanding.
Comments
- 
            Hello, The biggest benefit you will see when changing to SiC compared to an IGBT in this application is a dramatic reduction in switching losses. This will allow you to use a smaller module and smaller heatsink solution compared to an IGBT approach. You can also reduce the dead-time to somewhere in the 350ns-1000ns range depending on your gate drive which can reduce distortion in the output current. We have created a reference design that may be of interest to you. Take a look at our 300kW inverter design at the link below: Let me know if you have any additional questions. Thanks, Adam 0
- 
            Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further. 0