spice grid file of CAS480M12HM3
hello all
When I refer to the spice grid file of CAS480M12HM3, I have questions about some parameters. What is the meaning of Vthfwd and RTJ? Refers to the threshold voltage and on-resistance?
Looking forward to your reply
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hi Emma,
These parameters refer to changes in the on-state resistance and threshold voltage as a result of temperature changes in the junction. As the voltage in Tj (relates to temperature in deg C) changes, the Rds(on) and Vth will change based on this function. VthFwd and RTJ are defined in lookup tables further below in the model file.
Thanks,
Brian
1 -
hi,
Can it be understood that RTJ and VthFwd do not represent on-resistance and threshold voltage, but can only say that changes in RTJ and VthFwd represent changes in on-resistance and threshold voltage?
Looking forward to your reply
0 -
Yes, that is correct.
0 -
I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
Blake
0