Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Estimation of maximum dV/dT for safe operation

Options
Arshith
Arshith Contributor Level 1
edited January 2025 in Discrete Products

I have designed 20kw interleaved boost converter for which I am using C3M0040120k1 . The voltage rise time will reach 800V @ 14ns . I want to know how to estimate (from datasheet) the safe dv/dt inorder to avoid latching of internal BJT and failure.

I want to avoid using snubbers nor larger turn -off resistor for slow turn off.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • FrankWei
    FrankWei Wolfspeed Employee - Contributor Level 2
    Options

    Hello Arshith,

    The maximum dV/dt rating of Wolfspeed C3M SiC MOSFET is 100V/ns. 800V/14ns= 57V/ns average. You can try to capture the Vds waveform to check the actual dV/dt stress. normally you can find the max dv/dt @ 30% to 70% of the Vds. you can also tune the gate resistors to adjust the dV/dt.

    not sure whether I answered your question. Thanks

    Regards,

    Frank Wei

    Arshith
  • FrankWei
    FrankWei Wolfspeed Employee - Contributor Level 2
    Options

  • Arshith
    Arshith Contributor Level 1
    Options

    Thanks for the information.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.