Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Troubleshooting Connection Issues with NXP Control Card PC-Based GUI for SpeedVal Kit

Options
biruka
biruka Contributor Level 1
edited February 2025 in Discrete Products

I have purchased the following components:

Wolfspeed Motherboard: MOD-MB-HB-0900V-40A
Wolfspeed Power Card: MOD-PWR-MM-C3M0016120K
Texas Instruments Gate Driver Card: UCC21750QDWEVM-054
Texas Instruments Controller Card: TMDSCNCD280039C

After configuring and building the MPPT connection and selecting the correct COM port, I attempted to use the NXP control card PC-based GUI for the SpeedVal Kit. However, I am unable to establish a connection; the connection indicator in the GUI does not turn green.

How can I troubleshoot or resolve this issue?

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 2
    Options

    Greetings:

    You mentioned that you purchased the TI controller card but then you said you attempted to use the NXP controller card. The NXP and the TI controller cards each have their own firmware which must be downloaded and flashed before you can connect to the GUI.

    The flash instructions and firmware are all available from the Speedval website linked below.

    https://www.wolfspeed.com/products/power/speedval-kit-modular-evaluation-motherboards/speedval-kit-half-bridge-motherboard/

    Julius R

  • biruka
    biruka Contributor Level 1
    Options

    Dear Julius,
    Thank you for your reply. I have already downloaded the firmware, and it has resolved my issue.

    However, I have another question regarding the inverter. Is it possible to test the inverter in the GUI, similar to how we test the MPPT in the GUI?

    ~Biruk

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 2
    Options

    Single-phase and three-phase inverter modes are both supported by the three-phase motherboard (MOD-MB-3P-0900V-40A-N) and they can be controlled through the GUI.

    Julius

  • biruka
    biruka Contributor Level 1
    Options

    Dear Julius,

    I’m using the MOD-MB-3P-0900V-40A-N motherboard, which supports single-phase and three-phase inverter modes. However, I can only see the MPPT circuit in the GUI and cannot find any inverter settings. Could you guide me on where to access the inverter controls on GUI?

    Thanks in advance for your help!

    ~Biruk

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 2
    Options

    Greetings:

    Are you certain you have the 3P board? Your original post has the part number for the half bridge version. which doesn't support inverter mode. Inverter mode is currently only supported by the NXP control card (HVP-56F83783).

    Julius R.

  • biruka
    biruka Contributor Level 1
    Options

    Hi Julius,

    I have NXP control card (HVP-56F83783) too for a three-phase invertor.

    ~Biruk

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    edited February 2025
    Options

    Hi Biruka,

    Closing this thread as there is an active similar thread posted by you. If you have a follow up question, at a later date, please "Start a New Discussion".

This discussion has been closed.