Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Testing for Eon and Eoff

Options
David2023
David2023 Contributor Level 1
edited May 2025 in Discrete Products

Hello,

I have a question as below.

Which one is the standard test method, Figure 1 or Figure 2.

Figure 1 have very long pins and parasitic inductance.

BR

David
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
    Hello David2023,

    Generally, having short leads contributing to low parasitic inductance is desired. For our testing and characterization Figure 2 is used.

    However, in some designs long leads are unavoidable due to the mechanical assembly used. It may lead to higher ringing and lower switching speeds and therefore higher switching losses. This is a trade-off to keep in mind. Thank you!

  • David2023
    David2023 Contributor Level 1
    Options

    Thanks TBhatia.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.