Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Parasitic capacitance of CAB450M12XM3

Options
TKishi
TKishi Contributor Level 2

Have the min/max values ​​for Ciss, Coss, and Crss for the CAB450M12XM3 available?
The test conditions are as described in the datasheet and there are no problems.

Best Regard

T Kishi

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • sjjimenezc
    sjjimenezc Wolfspeed Employee - Contributor Level 1
    Options

    Hello,

    Thank you for your inquiry regarding the capacitance characteristics of the CAB450M12XM3.

    Please note that while the minimum and maximum values for Ciss, Coss, and Crss are not specified in our datasheet, we do provide typical capacitance values at 800 VDS, 100 kHz. For a more comprehensive understanding, I encourage you to review Figures 8 and 9 in the datasheet, which illustrate the capacitance versus voltage profiles in detail.

    If you have any further questions or need additional information, feel free to reach out.

    Best regards,

    Sergio J.

  • TKishi
    TKishi Contributor Level 2
    Options

    Hi

    Thank you for reply.

    Customer understand that Ciss, Coss, and Crss change depending on the VDS, but the customer would like to know how much they change at 800 VDS.This data is not available?

    Best Regard

    T Kishi

  • sjjimenezc
    sjjimenezc Wolfspeed Employee - Contributor Level 1
    Options

    Hi T Kishi,

    Unfortunately, we do not provide minimum and maximum values for Ciss, Coss, and Crss at 800 VDS. We only lists the typical values for these parameters under the specified conditions.

    Best regards,

    Sergio J.

Sign In or Register to comment.