C3m0075120K
how evaluate the Eon and Eoff in different voltage level, as the datasheet only provide the 400V and 800V Eon and Off chart
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hi lok,
Generally, it is assumed that the switching losses in a MOSFET scale linearly with the drain to source voltage. i.e. E(Vds=800) = E(Vds=600)*800/600.
This approximation is very accurate for small changes in voltage (e.g. 800 to 850V), but you can also extrapolate the slope between the two voltage points in the datasheet (which is the approach used by PLECS).
Let me know if you have any other questions!
Thanks,
Blake
0 -
thank you very much!!
0 -
Great, I'm glad I was able to answer your question.
I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0