CRD-30DD12N-K reference design : the control board (CLA funtion)
        
            Options        
            
        
Hello,
With respect to the reference design of CRD-30DD12N-K, I have a question on the control board.
The device of TMS320F28377D is employed as the DSP.
I wonder if the CLA function of TMS320F28377D is used for the firmware.
The CLA1 of cpu1 is configured and initialized in the firmware.
However it seems that the function of CLA1 is made inactive because the source codes in the Cla1Task2() and Cla1Task8() are made inactive with the comment context.
What functions were the Cla1Task2() and Cla1Task8() intended to provide for?
Thank you for your consideration.
With regards,
GKIM
0
            Comments
- 
            Hi GKIM, CLA function isn't used in this design, only CPU1. Thanks! 0
This discussion has been closed.