Bipolar output using SpeedVal Kit
I am trying to find out if there is any reason why I could not use the following SpeedVal Evaluation Platform configuration to generate a Bipolar output e.g. +800V to -800V and a sinusoidal waveform about 0V.
The EVAL-ADUM4146WHB1Z Gate Drive Module does support Bipolar HV Supplies for a H-Bridge.
See this example from the data sheet, obvously the EVAL board provides Dual Drivers for High and Low Side:
I hope to use the MOD-PWR-MM-C3M0075120J H-Bridge module and
connect HS+ to +800V and HS- to -800V, essentially like this:
I need to connect my PSU ground to the Mid-Point, as shown on the schematic for MOD-PWR-MM-C3M0075120J.
The Mid-point seems to be also called the Switch-Node in the user guide:
On the Motherboard, there is what looks like a screw terminal for the Mid-point.
So finally my question is, using the modules listed above, if I connect a Dual PSU, GND to the Mid-point, +800V to the HS+ (Bus+) and -800V to the HS- (Bus-), would this work? Is it recommend and what other issues might there be? Is there some jumper setting or other config that needs to change?
Many thanks
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello Ash2002,
Unfortunately the configuration you have proposed is not possible with a single SpeedVal Kit motherboard. Placing +800 on +Bus and -800 on -Bus would apply 1600V to the DC bus, which exceeds the voltage rating of the capacitors, and would put 1600V of stress across a 1200V MOSFET when the other device is turned on.
One method you could use to achieve a +/-800V peak sine wave output would be to use two motherboards configured as an H-Bridge to allow for a bi-polar output. Supplying both boards with an 800V bus using two 400V power supplies with the mid-point grounded would keep the motherboards and MOSFETs within their rated voltage and be capable of providing a +800 to -800V peak output to the load. A simplified diagram is shown below. Please let me know if you have any other questions.
Thanks,
Adam
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0