Question about usage of snubbers in CRD300DA12E-XM3
Hello Experts,
In the CRD300DA12E-XM3 inverter, we don't see the usage of any snubber capacitors across the Power modules.
Could you please shed some light on how the ringing is controlled?
Thanks
AK
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello AK,
The ringing is reduced by minimizing the parasitic inductance in the inverter's power loop. Starting with the module, the XM3 has a very low stray inductance of approximately 6.7 nH. Next, the system is designed to have high mutual-inductance between the DC+ and DC- layers through a tightly-coupled, laminated bussing structure. This mutual-inductance cancels out much of the self-inductance resulting in a low overall parasitic inductance seen by the system (roughly 10 nH total including the module & system).
The bussing design mates to the module in a unique manner as shown below by the red (DC+) and blue (DC-) bus bars, which eliminates the need for bends in the bussing structure and reduces the cost of the design.
The full cross-section including the DC-link capacitors and module internals is shown below.
We've also selected low-ESL capacitors to further minimize the stray inductance of the power loop. When care is taken in the design of the system with regards to minimizing parasitic inductance, a snubber circuit is not necessary as the overshoot and ringing is minimal.
Best Regards,
Austin C.
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0