How to change the Vth of a SiC MOSFET Ltspice model
 
            The technical article in wolfspeed knowledge center https://www.wolfspeed.com/knowledge-center/article/modeling-common-topologies-with-wolfspeed-silicon-carbide-mosfets/
simulates parallelling SiC MOSFETs with different Vth, that is Vth=2V and Vth=3V as figure below
I'm wondering how to change the Vth of a SiC Ltspice model, which parameter in the model should be changed or using other methods to simulate like that in Figure.6
Comments
- 
            Thank you for your post, it has been approved and we will respond as soon as possible. 0
- 
            Hi, In this instance, the e3 behavioral voltage source (from NET3 to ground) demonstrates the temperature-dependent threshold voltage. You can alter the value assigned here to fix to the Vth to a desired value. I hope this helps! Thanks, Zack 0
- 
            Thanks Zack, I have tried but it dosen't work, where can I alternate, just in the lib file or change which value in e3 or use spice order, I'll appreciate if you could give me an example. 0
- 
            just change in .lib file on e3 or use spice line code? 0
- 
            Hi, You'll need to adjust this value in the *.lib file. If you want to have access to adjusting it using the spice line you can declare a .param for the threshold voltage inside the *.lib file and access/modify it using the spice line editor. I updated the model for the C3M0016120D to reflect this change and put together a simple circuit that demonstrates how this works - please see the attached zip. You should be able to use the *.lib file in your designs without issue. Thanks, Zack 0
- 
            Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further. 0