Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Support of TI control card TMDSCNCD280039C for motherboard MOD-MB-HB-0900V-40A

Options
demosupen
demosupen Contributor Level 2
edited October 2024 in General

I want to use TI control card TMDSCNCD280039C for the motherboard MOD-MB-HB-0900V-40A. Unfortunately, the Speedval Graphical User Interface (GUI) only provides minimal options on the control. I am thinking of using the CCS(Code Composer Studio) and C2000Ware provided by TI to control the card TMDSCNCD280039C. Unfortunately, I did not find any resources for this. Can you provide the CCS source code or guidelines for this? Thanks in advance.

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • AAnders
    AAnders Wolfspeed Admin - Contributor Level 4
    Options

    Hello,

    Yes, the GUI is intended for basic power and dynamic testing, focusing on the gate drive and MOSFET testing. For more advanced controls, you will need to develop/modify the C2000 firmware. I will share the existing C2000 source code with you via email as a starting point.

    Thanks,

    Adam

This discussion has been closed.