Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

H-Bridge Question

Options
Doyle
Doyle Contributor Level 1
edited January 2025 in Module Products

I am hoping to run one of the H-bridge modules or to make an H-bridge using Wolfspeed products. However, I notice that there are only half-bridge driver modules available for purchase. Is it possible to use two half-bridge drivers such as the CGD1700HB2P-BM3 to control an H-bridge?

The H-bridge needs to support a DC bus of 1300 V or more. Any guidance here would be most appreciated.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4
    Options

    Hi Doyle,

    Yes, utilizing two half-bridge gate drivers to control a full-bridge is acceptable. The CGD1700HB2P-BM3 is able to support a bus voltage of 1300 V. The CGD1700HB2M-UNA is also a popular choice in a smaller form factor.

    Best Regards,

    Austin C.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.