H-Bridge Question
I am hoping to run one of the H-bridge modules or to make an H-bridge using Wolfspeed products. However, I notice that there are only half-bridge driver modules available for purchase. Is it possible to use two half-bridge drivers such as the CGD1700HB2P-BM3 to control an H-bridge?
The H-bridge needs to support a DC bus of 1300 V or more. Any guidance here would be most appreciated.
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hi Doyle,
Yes, utilizing two half-bridge gate drivers to control a full-bridge is acceptable. The CGD1700HB2P-BM3 is able to support a bus voltage of 1300 V. The CGD1700HB2M-UNA is also a popular choice in a smaller form factor.
Best Regards,
Austin C.
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0