25 kW FM3 Three-Phase Inverter
Hi,
I have already purchased two Wolfspeed inverters and I am currently using them. I have a couple of issues related to this.
- The purchased inverters are: 25 kW FM3 Three-Phase Inverters - CRD25DA12N-FMC, V1.2 01/2024. On the Wolfspeed website, the available CRD25DA12N-FMC_ALL_Design_Files are for V1.1. Can you please provide us with the newer version (V1.2) design files including the Altium, BOM, Gerbers, schematic, and the user guide pdf?
- Is there an encoder interface on the Wolfspeed board except for the resolver(J16)?
- We have the CCS code provided by Wolfspeed for CRD25DA12N-FMC. Is there a coder interface that we can use on this board or the control card.? Has this code been generated through auto-coding using a simulation platform like PLECS or Matlab? If that is so, can you please provide us that related PLECS or other Simulink model ?
Thank You!
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello Ujala_MG,
Thank you for your interest in this product. I answered your questions individually below.
- I attached the V1.2 files.
- The resolver is the only built-in mechanical feedback. There are also some spare ADCs and GPIOs that can be used to add additional sensor functionality.
- We only provide the CCS code. We do not provide a coder interface for the design.
Thanks,
Chris N.
0 -
Thank you for the given information!
Are the resolver inputs on the Wolfspeed board designed for a specific resolver model? If that so, what would be the resolver model?
Has the code been generated through auto-coding using a simulation platform like PLECS or Matlab? Can you please provide us with a PLECS/Matlab Simulink model that can be used for auto-code generation for the inverter?
Thanks!
0 -
Hello Ujala_MG,
By default, the resolver excitation signals are fixed and are optimized for 7 Vrms @ 10 kHz resolvers such as the Tamagawa TS2640N321E64.
The code was not generated using auto-coding. It was written directly in Code Composer Studio, so we do not have an auto-code generation model of the design.
Thanks,
Chris N.
0 -
Thank you!
Would you please let me know the J8 spare connectors' 5V power supply pin's current rating (supply current of the +5V pin)?
0 -
<1 A. The connector pin is rated for 3 A (datasheet), but the pin is powered from a 12V-to-5V DC/DC converter which is only rated for 1 A, and powers other circuitry on the board. We do not recommend trying to draw close to 1 A of current on this pin since it may cause an unreliable 5 V rail, which powers critical circuitry on the board.
Thanks,
Chris N.
0 -
I want to use this 5V spare pin to connect a hall-effect sensor which requires a 5V voltage supply and , a 7 to10 mA current supply. Will this be possible with the 5V spare pin on the Wolfspeed board?
Thanks!
0 -
Yes.
Thanks,
Chris N.
0 -
Can you please let me know the maximum and minimum voltage levels of the resolver Sin+, Sin-, Cos+, Cos- pins can handle?
Thanks!
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0