Aux Board
Hello,
In the CRD60DD12N reference design, the 6.5V voltage generated on the aux board is not reaching the main board. Upon tracing this path, we found that this voltage is not being generated by the aux board. Additionally, the CON2 (J344) connector has been left open, which prevents the isolated voltage measurement IC, op-amps, and gate driver ICs on the driver board from receiving 5V power.
Could you please help us with this issue?
Thank you
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hi Nkara,
Actually, the J344 was connected to the winding (2,8) of T12 via two jump-wires on the Aux power board,
due to the creepage limitation. Please refer to the following image.
0 -
Thank you very much for your reply. This was helpful for me
0