Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Aux Board

Options
nkara34
nkara34 Contributor Level 1
edited February 2025 in General

Hello,

In the CRD60DD12N reference design, the 6.5V voltage generated on the aux board is not reaching the main board. Upon tracing this path, we found that this voltage is not being generated by the aux board. Additionally, the CON2 (J344) connector has been left open, which prevents the isolated voltage measurement IC, op-amps, and gate driver ICs on the driver board from receiving 5V power.

Could you please help us with this issue?

Thank you
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
  • Hzz
    Hzz Wolfspeed Employee - Contributor Level 1
    Options

    Hi Nkara,

    Actually, the J344 was connected to the winding (2,8) of T12 via two jump-wires on the Aux power board,

    due to the creepage limitation. Please refer to the following image.

    nkara34
  • nkara34
    nkara34 Contributor Level 1
    Options

    Thank you very much for your reply. This was helpful for me

This discussion has been closed.