Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Open gate source connection

Options
Aradhya
Aradhya Contributor Level 1
edited July 1 in Module Products

Can I give gate source signal from the gate driver to one of the gate source pair and leave the other pair open for the inverter design? If not then please let me know what can be the possible issues?

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hello Aradhya,

    Can you please confirm you're referring to the XM3 module family, CAB320M17XM3 correct? Thanks!

  • Aradhya
    Aradhya Contributor Level 1
    Options

    Yes it is correct

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4
    Options

    Hi Aradhya,

    The two gate pins and the two source pins are connected internally in the XM3 module. You have the option to only supply the VGS signal to 1 pair of pins and the module will function. For the best performance and reliability, we recommend that both pairs of pins are utilized.

    Best Regards,

    Austin C.

  • Aradhya
    Aradhya Contributor Level 1
    Options

    Will the open pin be affected by some unwanted signal

This discussion has been closed.