Selection of the suitable gate driver module for Sic Mosfet
Recently I have purchased the C3M0016120D SiC MOSFET. The static operation gate-source voltage of the device is -4/+15 V. What is the suitable gate driver module, that gives highest level of modularity and compatible voltage levels? At the input I want to feed ingle ended 3.3-5 volt PWM logic.
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello Ankush,
If you're looking for a single-channel and single ended gate driver module, you can consider CGD15SG00D2 to use with C3M0016120D.
If your application is using the device in half bridge configuration, you can also consider a list of gate drive cards below:
However, all these gate drive cards use differential signals to enable high noise immunity. If you prefer to work with single-ended signals, CGD12HB00D transceiver board can help you achieve the conversion.
For more information on gate drivers, please check out this page:
If you're currently at an evaluation phase with C3M0016120D, you can also check out are SpeedVal Modular Evaluation Platform that makes evaluating devices, gate drivers, control cards etc. very easy and all the gate driver options I listed above are also compatible with that kit.
Thank you!
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0