Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD-5FF0912P Frequency

Options
TXBorne
TXBorne Contributor Level 1
edited October 2025 in General

Per customer, “Is the SiC MOSFET half bridge module inverter (CRD-5FF0912P) working in 1MHz or switching frequency is 1MHz?? “
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
    edited September 2025
    Options

    Hello TXBorne,

    CRD-5FF0912P is an old evaluation platform that was meant for Clamped Load Inductive or Double Pulse Dynamic Test. What I believe it means by the language of being able to switch at "2MHz" is the total pulse width for the CIL test can be as low as 0.5us. This board is not meant for continuous operation at a 2MHz switching frequency and we no longer support this board.

    Please refer to our new evaluation platform for discrete devices SpeedVal™ Kit Modular Evaluation Platform.

    TXBorne
  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.