Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Inductor for CRD25DA12N-FMC-AFE

Options
tjdonne
tjdonne Contributor Level 1
edited November 2025 in General

Hello,

Is there a standard inductor to use for L1-L3 for CRD25DA12N-FMC-AFE. The listed inductor in the BOM "SUNLORD ARCDC704772A301N1B" does not seem like a readily sourceable part.

Alternatively, does this design use a standard footprint so an alternative P/N could be used?

Thanks in advance!
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
    ChrisN Wolfspeed Employee - Contributor Level 4
    Options

    Hello tjdonne,

    The inductors used for this AFE are the same ones from Wolfspeed's discrete 22 kW bi-directional active front end (CRD-22AD12N). There are more details about the magnetics on the landing page for that design if you navigate to Technical & Sales Documents CRD-22AD12N Magnetics Specs. This download provides technical details about the ratings and dimensions of the inductors. While we do not have an alternative part number already tested, this should hopefully enable you to find a suitable replacement.

    Thanks,

    Chris N.

    tjdonne
  • ChrisN
    ChrisN Wolfspeed Employee - Contributor Level 4
    Options

    Hello tjdonne,

    I'm hope that answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Thanks,

    Chris N.

This discussion has been closed.