Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Request for PLECS Thermal models of ECB2R1M12YM4 and ECB1R6M12YM4

Options
gSu
gSu Contributor Level 1
edited February 6 in Module Products

Hello,

This is a request for PLECS thermal models of the these 2 Gen-4 6-pack modules: ECB2R1M12YM4 and ECB1R6M12YM4.

Thank you.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • BlakeNelson
    BlakeNelson Wolfspeed Employee - Contributor Level 3
    Options

    Hi gSu,

    Here are the two models requested in the "MOSFET with Diode" format:

    If you would like to use the legacy format (separate MOSFET and body diode models, which is generally not recommended), we do include it in our download: All PLECS Device Models

    Occasionally, Chrome will cash a previous version of the download, but opening the link in a private / incognito window can be used to eliminate this issue.

    Let me know if you need anything else!

    Thanks,
    Blake

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 4
    Options

    Hello gSu,

    I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Thanks,

    Chris N.

This discussion has been closed.