Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD-03600AD065E firmware not match

Options
USER_KE
USER_KE Contributor Level 1
edited December 2025 in General

hello tech team:

I'm working with CRD-03600AD065E-L reference design,but i found the firmware you provide not match the Schematics ,the firmware is 1ph3interleaved totem pole topology。Could you help me corrected?thank you.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • SGhosh
    SGhosh Wolfspeed Employee - Contributor Level 1
    Options

    Hello,

    Thank you for your inquiry. We appreciate your interest and want to clarify the concern.
    The CRD-03600AD065E-L firmware was modified based on the TI reference design (TIDA 01604). While the TI design incorporates their PowerGUI firmware, our approach utilizes a CAN bus in conjunction with the firmware code to operate the hardware.

    To clarify, the code is accurate and specifically tailored for the CRD-03600AD065E-L model. However, please note that the PowerGUI referenced in the forum image is outdated, and the current firmware code is not associated with it. For detailed operating instructions, I encourage you to refer to the user guide, which should provide clear guidance on using the provided code and CAN communication with the CRD-03600AD065E-L.

    If you have any further questions or need additional assistance, please don’t hesitate to reach out.

    Thanks,

    Sumana G

    USER_KE
  • USER_KE
    USER_KE Contributor Level 1
    Options

    Thank you for your prompt reply. I have noticed the modification of the source code based on TIDA 01604(from 3phase interleaved PFC to 1phase PFC)but i have some doubts,i don't understand: why the phase shift of high-fre FET relative to low-fre FET is 120 degrees still?

    I will continue to monitor your products and applications,thank you.

  • SGhosh
    SGhosh Wolfspeed Employee - Contributor Level 1
    Options

    Thank you for your inquiry. I’d like to clarify that the low-frequency PWM is generated at line frequency, which is not connected to this part of the code. The Base 4 PWM functions as a slave generator, deriving its reference from the Base 1 master PWM. In essence, Base 4 represents the high-frequency PWM signal, while the low-frequency signals are generated by the AC_FREQ ramp generators.

    For further details on how the high-frequency output pulse mode is selected, I suggest looking into the epwm.h file, which should provide a more comprehensive understanding.

    Thanks,

    Sumana

  • SGhosh
    SGhosh Wolfspeed Employee - Contributor Level 1
    Options

    I hope that answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Thanks,

This discussion has been closed.