Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CGD1700HB2P-BM2 DCDC converter replacement for different VgsH and VgsL

Options
littleBlue
littleBlue Contributor Level 1
edited February 17 in Module Products

Hello,

is it possible to change isolated DCDC converter and the gate driver evaluation board CGD1700HB2P-BM2 (PST1 and PST2 from schematics), from MGJ2D122005SC (+20V/-5V) to MGJ2D121509SC (+15V/-8.7V) and what would be required to change in addition to DCDC converter?

Best regards.
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
    Hello littleBlue,

    Yes, you can replace the DC/DC converters on the CGD1700HB2P-BM2 gate driver with different isolated DC/DC converters in the same case/package (7-SIP with 5 Leads). This is common when users want to evaluate the module performance with different gate voltage biases. However, when changing the converters, it is still important to consider the following:

    • The converter must have suitable isolation for the target bus voltage since it bridges the isolation barrier (see PRD-09301 for more information). The MGJ2D121509SC converter you identified is a suitable replacement from an isolation standpoint.
    • Operating SiC power modules outside of the rated gate voltages can degrade the lifetime. Many BM2 power modules (which this gate driver is design to support) such as the CAS300M12BM2 are rated for output gate voltages of -5 V / +20 V (with maximum ringing/overshoot ratings of -10 V / +25 V). The MGJ2D121509SC does not create the correct static output voltages, so this should be considered when deciding whether to make the modification.
    • If you want further control over the negative gate voltage, you can depopulate RB14 and RB15 then populate UB1, UB2, and their surrounding circuitry in order to adjust the negative gate voltage. The default resistor values are selected to create a -4 V rail, but the values can be varied to fine tune the negative output voltage.

    Thanks,

    Chris N.

    littleBlue
  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 4
    Options

    Hello littleBlue,

    I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Thanks,

    Chris N.

This discussion has been closed.