Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD-25BDA6512N-K Firmware download issue

Options
bsli
bsli Contributor Level 1
edited May 2025 in General

I was trying to download the firmware via Request Separately on the Product Page of the CRD-25BDA6512N-K 25kW T-type Inverter, but ran into errors requesting reference_design every time after I provide my information in the form and agree on terms and conditions. I wonder why this happens.
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
    edited May 2025
    Options

    Hello bsli,

    We're unable to support your request for the firmware of CRD-25BDA6512N-K. We only support the firmware with the purchase of this design and right now the design isn't available for purchase.

    You can refer to TI's TIDA-01606
    11-kW, bidirectional three-phase three-level (T-type) inverter and PFC reference design firmware which is the original firmware modified for CRD-25BDA6512N-K. Thank you!

    https://www.ti.com/tool/TIDA-01606

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. If it did, please click on "This question has been answered - Close Discussion" . If you have a follow up question, at a later date, please "Start a New Discussion"

This discussion has been closed.