CRD-22AD12N at lower power & voltage, higher frequency
Options
Nathan
Contributor Level 1
I would like to utilize the CRD-22AD12N for rectification and conversion of a variable speed 1kW generator operating between 20Vrms-72Vrms input and 20Hz-200Hz.
Be able to driving the generator (as a motor) at 72Vrms would also be desirable.
Would this module be able to support my requirements?
Tagged:
0
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
I'll also add that the output bus voltage is a parameter we can vary, but ~150V or less would be ideal.
0 -
Hello Nathan,
Sorry, the CRD-22AD12N is not able to support the application as you mentioned, this demo is only able to operate in the specifications that were listed in the User Guide PRD-02282 as below:
Thank you!
0
This discussion has been closed.