Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CAS175M12BM3 about temperature measurement

Options
TKishi
TKishi Contributor Level 2
edited August 20 in Module Products

Customer has question. Please coperate me.

Customer would like to measure the heat generation temperature of the CAS175M12BM3.
Could you please confirm the following two points?

  1. Where to attach the thermocouple to the heat sink.
  2. How to calculate the junction temperature from the measured.temperature

best regard

T Kishi

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • TKishi
    TKishi Contributor Level 2
    Options

    Hi

    When can we expect a response to this matter?
    A customer has requested a response, so please respond.

    Best Regard

    T Kishi

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4
    Options

    Hi T Kishi,

    In general, it is not possible to attach a thermocouple to a heatsink and accurately determine the junction temperature of the die in a power module. Significant characterization must be completed to create a mapping of heatsink temperature to junction temperature across various system parameters including flow rate and ambient temperature. This translation between heatsink temp and junction temperature is unique to each customer's end system; therefore, it is not a parameter that we can provide.

    Please refer to the Thermal Characterization Methods and Applications App Note on our website for a thorough explanation of determining the junction temperature of a power module.

    https://assets.wolfspeed.com/uploads/2024/02/Wolfspeed_PRD-08376_Thermal_Characterization_Methods_and_Applications_Application_Note.pdf

    Best Regards,

    Austin C.

  • TKishi
    TKishi Contributor Level 2
    Options

    Hi Austin

    Thank you for your reply.
    Is it correct that the most effective way to measure the Tj of a module like CAS175 is to use the body diode?

    Best Regard

    T Kishi

This discussion has been closed.