Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Simulation model for C3M0900170J

Options
ecksthom
ecksthom Contributor Level 1

Hello,

I have a question regarding the simulation model of the "C3M0900170J" MOSFET.

For my design, I would like to simulate the circuit with the C3M0900170J in SIMPLIS.
The reason is that other components of the circuit are only available in SIMPLIS.

Thus, I would like to know if the simulation model of the C3M0900170J can be made available for SIMPLIS.

Thanks in advance!

Best regards,

Thomas

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ecksthom
    ecksthom Contributor Level 1
    Options

    Thank you!

  • Mhusain
    Mhusain Wolfspeed Employee - Contributor Level 2
    edited September 3
    Options

    Hello,

    Thank you for contacting us! Here is the model that is compatible with SIMetrix. If you have any further questions, please feel free to reach out.

    Thanks!

    ecksthom
  • ecksthom
    ecksthom Contributor Level 1
    Options

    Hello,

    Thank you very much for your help!

    I tried to install the model and use it in SIMPLIS.

    Unfortunately, it only works for me in SIMetrix and not in SIMPLIS.
    Is there anything special I have to do? Does it work in SIMPLIS for you?

    Thanks,
    Thomas

Sign In or Register to comment.