SpeedVal Kit 3phase-board:SCP triggered when switching on upper device

Dear all,
I’m currently using the following products for my research project:
MOD-MB-3P-0900V-40A-N
EVAL-ADUM4146WHB1Z
MOD-PWR-MM-C3M0032120K
I didn’t use the control card — instead, I generate the PWM signals externally.
In my setup, I only need to produce a single voltage pulse. However, I’ve observed something strange:
—When I use the upper device evaluation configuration and switch on the upper device, the gate driver’s red LED turns on, indicating an SCP (short-circuit protection) event.
—When I use the lower device evaluation configuration and switch on the lower device, no SCP error occurs.
I would like to understand why SCP is triggered only when switching the upper device. Could this be related to the measurement configuration, gate driver reference, or bootstrap/isolated supply setup?
Any suggestions or explanations would be greatly appreciated. Thank you very much!
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0