Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

transformer for CRD60DD12N-GMB

Options
erikiverson
erikiverson Contributor Level 1

Is there any suggested part choices for the transformer of reference design

CRD60DD12N-GMB ? It isn't listed in the BOM or design files.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ChrisN
    ChrisN Wolfspeed Employee - Contributor Level 4
    Options

    Hello erikiverson,

    The transformer was a custom solution that we wound internally with a magnetizing inductance of ~100 µH and a leakage inductance of ~5 µH. It used Ferroxcube E100/60/28-3C94 ferrite E cores with AWG4-equivalent Litz wire. We’ve been working with our magnetics partners to develop a transformer solution for public release and expect to have more details released on the design in the next few months!

    Thanks,

    Chris N.

Sign In or Register to comment.