Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD25BDA6512N Choke/Inductor Selection

Options
jpeverill
jpeverill Contributor Level 1
edited November 2025 in Discrete Products

I am building some CRD25BDA6512N for evaluation to start off a new design. The line choke components (L1_1, L1_2, L1_3) and (L5_1, L5_2, L5_3) are not specified. They appear to be stacked on the same footprint? I'm not clear if these are two different parts intended or two different chokes wound on the same core? Are there specifications for what was used to build the reference boards? The BOM just says "Line Choke, 125uH, 100kHz, 6.5mOhm DCR" and "Inductor, 131uH, 20kHz, 7.5mOhm DCR". I am aware that there is another EMI filter that is referenced and suggested for production designs but I would like to start with just building the reference design.

Thank you!

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

    jpeverill
  • Hzz
    Hzz Wolfspeed Employee - Contributor Level 1
    Options

    Hello,

    That just intended to be compatible with the two types of inductors from two different vendors, finally, we just used the following component from POCO for this design. thanks.

    Ensider
Sign In or Register to comment.