Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Unexpectedly Slow Vsd Settling Time (300-400ms) During Tj Measurement on C3M0021120K

EEhcy
EEhcy Contributor Level 1

Dear Sir or Madam,

I am currently working on a project to measure the junction temperature (Tj) of a Wolfspeed SiC MOSFET (Q1: C3M0021120K) by monitoring the forward voltage drop (Vsd) of its body diode with a pre-calibrated K-factor. However, I've encountered an unexpected and very slow Vsd settling phenomenon that I'm hoping to get some insight on.

Measurement Setup and Procedure:

My test circuit is designed to first heat the DUT (Q1) and then quickly switch to a low-current measurement phase. The schematic is attached below.

  • DUT (Q1): C3M0021120K
  • Measurement Switch (Q2): IMBG120R034M2HXTMA1 (Infineon CoolSiC™)
  • Sense Current: 100mA constant current source
  • Vsd Measurement: A differential amplifier measures the voltage directly across the source and drain of Q1, which is then fed to an isolated amplifier and an ADC.

The measurement sequence is as follows:

  1. Heating Phase: Q1 is turned ON, and a DC power supply provides a constant current of 10A through its channel to heat the die.
  2. Transition and Measurement Phase:
    • The 10A heating current is stopped, and Q1 is turned OFF.
    • After a delay of 100µs, the measurement switch Q2 is turned ON, injecting the 100mA sense current through the body diode of Q1.
    • After an additional 100µs delay (total of 200µs from Q1 turn-off), the ADC begins its first measurement of the Vsd.

The Problem I'm Observing:

I expected the Vsd reading to be relatively stable, reflecting the die temperature at the moment of measurement.

However, even with the 100µs settling time allowed after current injection, I am observing a very slow transient. The initial Vsd reading is significantly higher than the final value, and it takes approximately 300-400ms for this voltage to decay and settle.

As shown in the attached oscilloscope captures:

  • Capture 1 (Zoom Position: 195µs): This corresponds to the very beginning of the ADC acquisition phase. The mean Vsd is measured at 1.84V.
  • Capture 2 (Zoom Position: 8.81ms): After just a few milliseconds, the mean Vsd has already dropped to 1.76V, and this downward trend continues for hundreds of milliseconds before stabilizing.

My Question:

What could be the physical mechanism behind this long (300-400ms) Vsd settling time, given that the measurement starts 100µs after the sense current has been applied?

A duration of several hundred milliseconds seems too long for a typical die-level electrical or thermal transient. Is this a known characteristic of SiC MOSFET body diodes, perhaps related to charge trapping/de-trapping or a more complex thermal effect within the package? Or could there still be an artifact from my measurement circuit that I am overlooking?

I would greatly appreciate any insights, suggestions, or similar experiences the community could share. Thank you in advance!

image.png image.png image.png
Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 3

    Greetings:

    I have some questions about your circuit schematic.

    1. When Q1 is turned off, what voltage is applied gate to source?
    2. You say you are measuring VSD across Q1 but the schematic shows the differential amplifier measuring across the combination of Q1 and Q2. Can you clarify?
    3. If Q2 is inside the sensed voltage measurement, how much voltage (gate to source) are you gating Q2 with?

    Julius R

Sign In or Register to comment.