Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Simulation

Sahaja
Sahaja Contributor Level 1

Dear Team,

Issue with the junction Temperature value is not meeting the calculations it is more than 23degree, kindly check the data and revert. calc is around 130's

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Mhusain
    Mhusain Wolfspeed Employee - Contributor Level 3

    Hello Sahaja,

    Thank you for reaching out. I believe I've identified the issue. In your calculation, it seems you considered only the thermal interface impedance (the MOSFET grease resistance, Rth,ch, which you set at 0.44 °C/W). This only accounts for the temperature difference between the heatsink and the case.

    To accurately calculate the junction temperature, you also need to include the junction-to-case thermal impedance, which is approximately the same, at 0.44 °C/W for this device.

    Using these values, the junction temperature can be calculated as follows:

    • Rth junction to case (included in the device model) = 0.44 °C/W (approximately)
    • Rth case to heatsink (MOSFET grease resistance Rth,ch) = 0.44 °C/W
    • Power loss in the MOSFET = Switching loss + Conduction loss = 52.25 W
    • Delta temperature = (0.44 + 0.44) * 52.25 = 45.98 °C
    • Heatsink temperature (Heat sink model: Fixed) = 90 °C
    • Junction temperature = Heatsink temperature + Delta temperature = 90 + 45.98 = 135.98 °C (approximately)

    For more information on transient thermal impedance and its role in calculating junction temperature, please refer to our Application Note: "Introduction to Pulsed Current Safe Operating Area."

    Let us know if you have any further questions!

    Regards

Sign In or Register to comment.