Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Use DSP28335 to drive CGD1200HB2P-BM2

SilvaDeng
SilvaDeng Contributor Level 1
edited January 28 in Module Products

I am using the DSP28335 chip to input PWM signals into the CGD1200HB2P-BM2. However, the CGD1200HB2P-BM2 can only receive differential signals. What chip should I choose to convert a single-ended 3.3V signal into a 5V differential signal? Is there a typical circuit for the CGD1200HB2P-BM2 device?

Comments

This discussion has been closed.