Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CPW5-1200-Z050B

Options
BGY
BGY Contributor Level 1

Hello!

I am currently working on the parallel simulation circuit for the internal chips of the module. The official website does not provide the LTspice model and .lib file for the Schottky diode of model CPW5-1200-Z050B. Could you please provide these two files?

Thank you very much!

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Mhusain
    Mhusain Wolfspeed Employee - Contributor Level 3
    Options

    Hello,

    Thank you for your inquiry regarding the LTspice .lib file for the Schottky diode CPW5-1200-Z050B. Unfortunately, this device is now considered obsolete. However, you can use the alternate part CPW6-1200-Z050A, for which I have attached the LTspice model and symbol here.

    If you have any further questions or need additional assistance, feel free to ask!

    Regards

Sign In or Register to comment.