Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Device Orientation in Reel

GustavoR
GustavoR Contributor Level 1
edited June 16 in Discrete Products

I would like your help to confirm what is the device orientation within the reel.

C6D10065G-TR

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4

    Hi GustavoR,

    The Power Product Packing & Shipping Reference Guide is intended to include the orientation of the G package in the tape & reel. Based on the image for the G package from that document, I see that it's not explicitly obvious which direction the package is inside the reel. The leads are located in the thin section and the body of the part is located in the wider section. I've included an example image of the TO-263-7L below, which matches the reel orientation for the G package.

    image.png J2 Package in Tape & Reel.jpg

    Best Regards,

    Austin C.

This discussion has been closed.