Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

LTSpice part format

billvolts
billvolts Contributor Level 1

I am trying to model a WolfSpeed MOSFET with the ADP1071 controller

in LTSpice XVII. It is not obvious from the MOSFET data what LTSpice

is looking for as the start of the data file. The WolfSpeed model

does not start with the word "Model" and LTSpice reports "Can't read C3M0065090D"?


I included a .TXT file of the C3M0065090 in the same directory as my project.

I entered the InstName as M1 and the Value as M1_C3M0065090D in the Component Attribute Editor.

I also included the part in the schematic page as .include M1_C3M0065090D.

The Wolfspeed part has two additional pins that I am not using since

the ADP1071 does not use them.

An example of using a Wolfspeed SiC MOSFET would be useful.

This discussion has been closed.