Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Inconsistency Between C3M0120090J datasheet and SpeedFit 2.0 Design Simulator for Switching Loss Cal

Efecan
Efecan Contributor Level 1

Hello,

As a company we use your SpeedFit 2.0 Design Simulator in Wolfspeed website. While simulating, we encounter with following problem.

Here, we use C3M0120090J SiC Mosfet in the circuit. we take gate resistance(Rg) of the transistor as 10 ohm in the simulation. Also, we enter below inputs for simulation in 25 Celcius. (400V, 15A)

image.png

After input stage, we get following results at the end of simulation. Switching power loss for all four SiC Mosfets is around 21W as you can observe.

image.png

When we look at the graph from C3M0120090J SiC Mosfet datasheet, we see that when Rg=10 ohm switching energy loss is around 50 uJ for one transistor. When it is multiplied by 250kHz switching frequency, 12,5W switching power loss is obtained for one transistor. As a result, for H-bridge circuit with 4 transistor above, total switching power loss should correspond to 50W according to datasheet. However, it is obtained as nearly 21W in the simulation. We wonder why inconsistency occurs in that situation. If you have any opinion for that problem can you explain?

image.png

Thank you for your consideration.

Tagged:
This discussion has been closed.