Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Measuring SiC MOSFET current in LTspice

Przemek
Przemek Contributor Level 1

Hello,

I am trying to do some double pulse tests in LTspice with models of SiC MOSFET transistors available to download on Wolfspeed site. However, when I am adding different transistors I am not able to measure their current (at the drain or source pin). I tried 2-gen MOSFET (C2M0025120D), 3-gen MOSFET (C3M0015065K) and bare die (CPM3-1200-0013A). I am adding these models by .lib SPICE directive. If I put in that place default MOSFET from LTspice library then everything is ok. I want to ask if there is no possibility to measure this current or am I doing something wrong? Of course, I could add a small series resistor to the transistor but I would prefer to measure transistor current without additional elements. Thank you for answer.

Przemek

Tagged:
This discussion has been closed.