Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Setup of thermal cycling testing

MinC
MinC Wolfspeed Employee - Contributor Level 2
edited October 2022 in Discrete Products

Hi Wolfspeed

Got one question from customer for the setup of thermal cycling testing in qualification & reliability report. is this devices soldered on the PCB or just a bare device only?

The reason for this question is customer is doing one evaluation for the mechanical stress to plastic body during the high/low temperature cycling testing. it will be great if you can provide Coefficient of thermal expansion, material yield strength, Young's modulus and Poisson ratio for our leadframe(footprint).

Leadframe.png


Thanks.

Mason

Tagged:
This discussion has been closed.