The ground capacity of the CAS300M17BM2
        
            Options        
            
        
 
            
                
                    Fertmann                
                
                    Contributor Level 2                 
            
                        
            Hi,
I would like to enquire about the ground capacities of the CAS300M17BM2 module CD1 and CD2?
Many thanks in advanced,
Martin
            Tagged:
            
        
0
            Comments
- 
            Hi Martin, For the BM2 modules, the per-terminal baseplate capacitances (CD1, CD2, and C in the below image from the application note you referenced) are as follows: CD1 - 187 pF CD2 – 271 pF C – 103 pF Please note that these values are from impedance analyzer measurements of a single module. The values for any individual BM2 module may vary slightly. Thanks, Brian D 0
This discussion has been closed.