CRD-30DD12N-K reference design : TMS320F28377D vs TMS320F28377S
Hello,
With respect to the reference design of CRD-30DD12N-K, I have a question on the control board.
The device of TMS320F28377D is employed as the DSP.
I wonder if TMS320F28377S can be used instead of TMS320F28377D for the control board.
They are pin-to-pin compatible devices.
I wonder if the dual cores of TMS320F28377D are all used for its control firmware.
If only the single core of TMS320F28377D is used for its control firmware, I suppose that TMS320F28377S may be able to be used instead of TMS320F28377D for the control board.
Thank you for your consideration.
With regards,
GKIM
Comments
-
Hi GKIM,
TMS320F28377D is selected for the control board, while only CPU1 is used for this design. Yes, the TMS320F28377S is available for a pin to pin substitutes. The firmware is configured for 28377D, some includes files maybe need to edit if warnings or errors happen. Thanks!
0