[FAQ-THERM-3] Can I directly solder TO-247 body to PCB or heatsink like surface mount devices?
Options
TBhatia
Wolfspeed Admin - Contributor Level 5
No. Usually there is a MSL (Moisture Sensitivity Level) rating for surface mount device to define the condition of the device before it is soldered to PCB. There is no MSL rating defined for TO-247 devices.
0