Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

[FAQ-M&S-3]How do get started using the SpeedFit 2.0 design simulator

SiC_Power_Admin
SiC_Power_Admin Wolfspeed Admin - Contributor Level 4
edited August 2021 in Device Models

When you navigate to the SpeedFIT simulator home page, the last tab called "User Guide" has helpful information on resonant converter simulation as well as thermal impedance data that can be used when starting a new design where the thermal performance of the heatsink is unknown.


image.png


Sign In or Register to comment.