Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Magnetics specs for a refrence design 60 kW

Kyre_44
Kyre_44 Contributor Level 2
edited January 2023 in Discrete Products

Hello

I'm not able to find much data on the magnetics design with the exception of 1 page that quickly coveres the main DC filter inductor, however its not clear , how the wire chosen would be able to handle large currents to achive 15 kW/phase - it seems like 18 of 25 AWG=~8 Amps current handling ability.

Also is the Delta I is the total ripple current for all inductors or is it for each phase or total ?

No data for the common Mode inductor,if you please share that too - Thanks


image.png


Tagged:
This discussion has been closed.