Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Using 600kW reference inverter to drive a single motor in parallel mode

RobertH
RobertH Contributor Level 1
edited February 2023 in Discrete Products

My group is currently using the 300kW reference inverter (CRD300DA12E-XM3) to power a unit under test, and after some development we are now up against the performance limits of that inverter. We have a 600kW dual-channel reference inverter on hand (CRD600DA12E-XM3). Question is, the documentation only speaks to using the two sides of the 600kW unit to drive two separate motors. Is there any experience or theory towards using both sides of the 600kW unit in parallel to drive a single motor past the limits of a single side?

Thank you!

Tagged:
This discussion has been closed.