Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

[FAQ-GPS-4] Can the body diode of a SiC MOSFET be used or do I need to add a parallel diode ?

SiC_Power_Admin
SiC_Power_Admin Wolfspeed Admin - Contributor Level 4
edited November 2024 in General & Product Selection

Yes, the body diode of a SiC MOSFET can be used for recirculation currents. For example, in a Totem Pole PFC high-frequency leg, an additional diode is not required due to the superior performance of the body diode

Sign In or Register to comment.