Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Gate source voltage measurement of SiC module

baiyujing
baiyujing Contributor Level 2
edited February 2023 in Module Products

Hello, I bought your half-bridge module CAB450M12XM3 and used CGD12HBXMP to drive it, but there is no measurement pin reserved for the gate source voltage(vgs) on the driver. How can I test the gate source voltage(vgs)? Is it necessary to connect two wires directly from the two welding points G and S on the drive board for measurement?

This discussion has been closed.